The DTM of the ABB Instrument ScanMaster FZC500 is available or can be used by the Device Manager of the 800xA?
My question is if someone know if the DTM of the ABB Instrument ScanMaster FZC500 is available or can be used by the Device Manager of the 800xA? If the answer is Yes I would like to know if exist a document where I can show that to the client? If someone have a project reference where this was implemented could be useful for me.
Answers
Hello Eurit,
the list of HART Devices supported with 800xA are listed in the link below.
Any other integration request with project name & complete details should be sent to DIC@in.abb.com
Link to Integrated Device List
Add new comment