IEC61850 Upload error
When trying to upload the scd file in Control Structure this error appears.
From the log:
Connecting to: IEC 61850 OP DA Server Instance[5] on the machine xxxxx
Connected to the OPC Server!
*
Starting Control Structure retrieve...........
Error: WA5\xxxxxxx
Error: Uploading failed, OPC Server is using different configuration
Error: Failed to do Control Structure retrieve
The upload operation has failed!
End log
We are using the same file when uploading in 800xA as we did when uploading in CET.
Anyone?
Or does anyone know who I should contact in this matter?
BR asp
Answers
You can add maximum of 4 server instances in 800xA for IEC61850 or even in more simplified language you can upload maximum of 4 scds. If you have added only 4 SCDs then please check the instance number of SCD import from CET & select the same instance number during SCD upload in 800xA. Delete the extra server instances rom 800xA.
Add new comment