How to create Faceplates
Answers
Greetings,
This question has asked before, please refer to that link:
Hi
Greetings.....
Just to add to Titus answer, following is the overview of creating a new faceplate:
- Create an Faceplate Aspect for the Object in the Object type Structure.
- Open the Faceplate Aspect in Config View. Configure the following:
•Layout Configuration of the faceplate geometry.
•Header Configuration of the object lock control and alarm control.
•Indicators Configuration of the Status and Navigation bar.
•Buttons Configuration of the Button area.
•Element Configuration of the faceplate element area.
•Online Help Configuration of the help files.
•Approval or unapproval of faceplates.
Refer Page 320 of 3BSE049230-510_E_en_System_800xA_Engineering_5.1_Process_Graphics.
Jope this will help you!
Best Regards
Sunny Khatri
Add new comment