SFC Step Time
Hi,
following settings in N section:
Step (StepNo := StepNo,
X := StepNo.X,
T := StepNo.T,
TMin := 5,
TMax := 15,
StepInfo => FromSFC.StepInfo1 );
All selections after the point are possible, only T can not be selected, in the step number is only X available.
Where is my mistake?
regards
nola2k
Voted best answer
make sure that in the CBM Editor, when the Step is selected, in the Tools Menu the Option "Step Elapsed Time" is selected
Add new comment