Is it possible to make ethernet redundancy in DigiVis?
In certain application, redundancy for ethernet is requried. Is there a way to acheive this?
Voted best answer
Since DigiVis operator station only supports one IP Adress, we can use 3rd party technology to achieve redundant DigiVis connection.
1. Can be done with dual-port NIC
2. Some NIC manufacturers developed a kind of Mixed-adapter teaming NIC, it can combine two network cards and specify one as primary, and this two network cards share one IP address.
1. Can be done with dual-port NIC
2. Some NIC manufacturers developed a kind of Mixed-adapter teaming NIC, it can combine two network cards and specify one as primary, and this two network cards share one IP address.
Add new comment