How to Get AC410_1 in 800xa Control Structure
We are not able to see the ac410(Safeguard system) database object in control structure after upload.
We need to get alarm when any one of the 24v DC supply is failed, and connection are done and wired to the SB171(Live 24_A and Live_24B).
Answers
i got the element under Local devices in control structure ( Local Devise graphical element aspect)
Add new comment