Is it possible to put a subnetmask and default gateway in a SYSTEM 6 DCU (symphony harmony) ? If so, How?
We saw the abb bootp server software (and other bootp server software) provides the option to make the bootp server supply the subnet mask and default gateway. Still we do not know if it is possible that the DCU gets and uses a default gateway and subnet mask. If this is possible, how does one configure this?.
Answers
Hi
Greetings..
I hope I got the question right for DCI Connectivity using Harmony DCU Controllers ot it is related to INIET800 or PNI800 node or the NCC.
If its for DCI - What is the need to give subnetmask and default gateway to DCU Harmony Controller. During Application building in Composer CTK, it asks only for following parameters:
- Node Number
- IP Address
- Mac Address
Your answer will help us to understand your issue in a better way.
Best Regards
Sunny Khatri
Add new comment