800M CPU tasks documentation
task load on an 800M - is it possible to have documentation of tasks as we could in the AC450 controllers - a document which explained briefly the task and could be checked using the ANPER command - so my question is - equivalent to ANPER on 800M and task description document
Voted best answer
As far as I'm aware, the AC800M is basically single threaded. Which is why EVERYTHING stops when the controller crashes.
So there is no equivant to ANPER, because there are no separate tasks performing different functions. There is only Cyclic and Overhead load.
Answers
Need to add a program and use Systemdiagnosis block .
This will tell the controller Loading and more detaisl
Source: 800xa
Add new comment