12 vs 24 hour clock for TIME01 element
An Integer Long DAT from an AC 450 is presented as a TIME01 element in a PG2 graphic display.
For most users/workplaces this is shown as time with a 24 hour clock, however one user/workplace has this shown as a 12 hour clock with AM/PM.
The presentation seems to be related to the user, but I can't find where this specific setting is. Anyone knows where I can find this setting to change from 12 to 24 h clock?
Thanks,
Tor Anders
Answers
It depends on Windows system setting, format is the same as the clock in the taskbar. For Windows 8.1: Control Panel > Region > Formats > Date and time formats. Workplace restart is needed after change.
Add new comment