Looking for a pump application preferrably for Compact Controller
must control two pumps, need it for a fresh water supply
Voted best answer
Found on ABB webpage interesting information about pump solution. Unfortuantly all in Swedish. Just type compact pump in the search engine on abb.com or follow attached link. There is a also a video about it. If you are interested I can try to find you a contact person in Sweden.
Answers
I am the engineer that wrote the Compact Pump application (in Swedish). It consists of an AC800M with I/O modules and the possibility to select between two different operator panels (820 or 835). The application supports up to 4 pumps controlled by relay, 4-20mA or fiber connection directly to an ABB Drive. All configuration is made using the operator panel. If there is any interest in an english version of this application please contact me. Thomas.Thunberg@se.abb.com
Kind regards
Thomas
Source: http://www.compactpump.se
check this app, solutions is available in both the languages.
by Gero@ABB Rank: 533 on 10/2/2011 4:29:11 AM | Like (0) | Report
i think an application exists in Swedish language
Add new comment