How to Set IP address for PM865 Controller
I know that we can set the IP address of PM865 using TK212 Cable and Laptop having Serial port.
But we have laptop without Serial port. Does anyone have any idea about how to use the USB port of Laptop to set the controller IP address?
Answers
Use a USB/COM converter.
Or if you know the IP address, use that as system identity, and set the new IP on COM1, then download.
Use a USB to Serial DB-9 RS-232 Converter to connect the TK212 to your PC and the standard Engineering Utility IPConfig. Be sure and check the docs with your converter cable because some of them do not work with USB 3 ports.
Add new comment