Export tag list from 800xA to Excel
How to export tag list and all alarm limit properties of my 800 X A project into an excel sheet. Plz show steps
Answers
It is pretty difficult to give you exact steps because you need to do slightly different things depending on how your project is programed. Anyway, all this is done with Bulk Data Manager.
You need to have the minimum installation of Engineering Studio ( which includes BDM ). Once BDM is installed then you can connect to your xA system and simply drag / drop the aspect properties you want to collect into the excel header and then drag/drop the object structure that you want to collect data from.
There are some very good examples in the Engineering Studio Basic Functions manual (3BDS011223) Section 3. This will show you how to configure the header in excel, filter the objects and export the data.
Add new comment