CI858 Parameters and Firmware
Hello,
Im communicating a DCS800 with a AC800PEC through Drivebus (CI858).
I have some doubts about how to download firmware on CI858. I have the manual, but it dont say anything especific about this topic.
I have a little aplication on Compact Control Builder, and below the CI858 I have the ABB Drive Template. I have comunication with the DCS800 but can't see any Drive status. I think that Im doing wrong on the ABB Drive Template settings. I did read the manual but dont understand well what is the real meaning of:
-Address of drive type in drive
-Dataset 1 ID
If I use the Engineered Drive do I have to donwload an especific firmware to the CI858??
Thanks!
Answers
i don't think that it's firmware but if you want to update the firmware it's smiple
right click on the controller in the controller builder
click remote system pop window will you will get your controller there then
click show firmware then you will find the window which show you the loaded firmware of the controller and communication cards and firmware present in the Compact Controller Builder if you want to upgrade then click all the check Box and Press Upgrade new firmware will be downloaded in the controller and Communication cards.
Please find the attached parameter of the drive which you can cross check
and Add Standard drive not the Engeering drive in the control Builder.
Add new comment