Why do DINTIS and DINTOS objects cause workplace to crash when code is generated in Function Designer?
I am integrating a Profibus device into 800xA 5.1 RU1k system. The project is using AC800M controllers (PM866) and CI854A Profibus masters. I can add DINTIS and DINTOS objects to a function diagram with dummy names and have the configuration generated properly. However, when I assign the proper IO names and descriptions and insert the signals into the Control Structure, generating configuration causes the Engineering Workplace to crash.
I need a workaround for this. Installing rollups or TC's is not in my scope and may not be permitted by the customer or engineering firm.
Answers
This question has not yet been answered.
Add new comment