Is it Possible to ping the Aspect Server from the Ethernet Port Switch installed in the Controller Panel
I have to install workstations in all the load centers, I'm thinking of laying CAT6 cable from the Ethernet Port Switch(D-Link DES-1016D) installed in the Controller Panel. The Plant Network is also connected to the same Switch.Is it possible to ping the aspect server from any of my laptop or the system must be connected in the domain.
Voted best answer
It doesn't depend on whether your laptops in the same domain or workgroup with 800xA aspect server or not.
You can ping aspect server from the laptop in case they both connected to the same switch and have the same TCP/IP protocol configuration.
Just open your LAN network adapter settings in the laptop, find TCPIPv4 properties and set there same with aspect server network subnet mask and IP address in the range of this mask (IP address must be but unique).
Add new comment