How to connect ACS800 to AC800M via RPBA-01 Profibus
Hello!
I would like to configure CBM for connect ACS800 to AC800M via RPBA-01 Profibus that I have already insert hardware on CI854 by using default libraries but I don't know parameters that I have to assign to hardware connection, if I select PPO type 5
Thanks
Charin P.
Answers
Was commented by Charin,
"Thank you everybody, I have already done for both sides. For drive side, I use default setting but change to PPO Type 5 and assign some required parameters to PZD Addressed. For DCS side, I insert ABBDrvRpbaCI854HwLib for HW Library and define variable as PP_ElementLib.ACS600Std_Par Type."
-Admin
Hi Charin,
To get basic information regarding communication to AC drive refer the document available in ABB solution bank. Examples are provided about configuration in drive parameters and in PLC side(AC500PLC). Hope it will be useful to you
by Govindaraj
Hello, Are u looking for solution in Drive side or in CBM configuration?
by itsashish_5june Rank: 6598 on 1/18/2013 12:31:26 AM | Like (0) | Report
Please explain more clearly that you need the parameter for CBM or Drive Parameter for configuration.
by charin Rank: 5159 on 1/18/2013 7:34:35 AM | Like (0) | Report
Thank you everybody, I have already done for both sides. For drive side, I use default setting but change to PPO Type 5 and assign some required parameters to PZD Addressed. For DCS side, I insert ABBDrvRpbaCI854HwLib for HW Library and define variable as PP_ElementLib.ACS600Std_Par Type.
Add new comment