Controller Password is Default - PM866
Hello,
Am getting a warning in Control Builder and this is visible in System status viewer as "Contrller Password is default". Am not sure the cause of this warning and am not having this for all the controller. Some one is mentioning its because if CI854 module.
I just wanted to get rid of this warning ... How to do !
Voted best answer
Hello,
If you have hardware modules like CI854 or CI871 in control builder, you will get an option to enable web server by right click on Processor module when control builder is in online mode.
If the above modules are exist and password is not changed from default, you will get this warning "Password is Default".
To eliminate this warning you can eanble the web server and change the password. After enabling web server, type the IP address of the controller in web browser and press enter. It will ask you for user name and password. If you are using 800xA 6.0, the user name and password are as given below:
User Name: service
Password: ABB800xA
Change the password in the above web browser, then the warning will be removed from the processor in control builder.
Answers
1. KeePass Password Safe
2. Keeper
3. Dashlane
4. LastPass
5. RoboForm
6. Sticky Password
7. Bitwarden
8. 1Password
9. TrueKey
Add new comment