averages on composer 6.0
so im trying to do aa 30 day average using FC165 averging on a set on of interlock, when to averge and when not to. the trouble is when i loose the interlock and want to averge the N value is not a same as it was before i lost the interlock. any help with this would be great.
Answers
Hi,
If Track doesn’t work for you by filling the average block buffer with the current value, what about ADAPTing S3 to a large number? This should effectively stall the FIFO buffer and the average calculation as well as preserving the individual buffer elements until you want to start to calculate an average again. When you are ready to start averaging, set S3 back to its normal value and the average calculation should kick off from where it stopped. The track input S4 would remain in normal during this time.
N.B. "should" implies that it sounds like a good idea but I havent tried it.
Cheers,
Alan
Add new comment