What is the difference between Function Diagram in 5.1 FP4 and Function Designer
Dear All,
Can anyone explain the main difference between nction Diagram in 5.1 FP4 and Function Designer.
And What are the advantages of using both.
Which is Best.
When to use.
How will these codes written in FD loads on the controller compare to conventional Programs (Using FBD, ST ,SFC).
How to use these FD in case of SIL applications.
Regards-
Mohan
Answers
FD will generate Diagrams in CBM so it is really the same. Loads are equal, at least for what i use (FBD, SCM <-> Diagrams).
There are some additional Functional Concepts in FD like Templates and Signal Allocation but it's generating Diagrams first which means that working directly in Diagrams is a bit faster.
Hi,
FD does not support SIL Applications
Add new comment