AC500 PM573-ETH How to make sure that the Ethernet configuration is correct
Hello,
I have configured a static IP address into a PM573-ETH with the keyboard. The PLC is connected to a rooter. How could I troubleshoot the PLC connection through the rooter (through a WAN). Does the ping command is enough to confirm that the connection is good. Do I have to configure something else in the PLC than the IP address, netmask and the default gateway. Do you have some tools to verify this connection.
Thank you, regards.
Answers
Hi
If you use Automation Builder tool, you can with Ip config tool / scan, verify any information about the IP adress of the cpu or eventually, modify how you prefer.
Add new comment