New Window popups behind existing window in operator workplace full mode.
Dear All,
New pop up window appears behind existing popup window in operator workplace (F11 Mode) but we reqiure in foreground always.
WR,
Lohith.D
Voted best answer
Hello,
it looks like you have Workplace Mode set to Windows mode, as you have to press F11. If it's set to Operator Mode, then all overlaps come over the Base display. If you want certain overlaps to be over other overlaps, then I think you have to create different aspect categories for graphic displays (or the kind of aspect you want as overlapped). Then you can define different view classes in Library structure per kind of overlap, with different Stacking order.
/Ronny
Answers
Hi.
One Solution is as below,
1) Go to Library Structure>>Expand Default View Class>>Expand ABB System
2) Click on Faceplate object to show its aspects in the aspects pane
3) Click on Default aspect>> Select Position at Cursor >> Select DataSource as Local and change the Boolean Value property to "YES"
4) Set Update Enable parameter and click OK
A faceplate will now open near the graphic element invoking it.
Note: Place operator workspace in full screen mode to enable pinning faceplates. Similar procedure is applicable to Graphic Display popup windows as well.
Regards
Rahil
Add new comment