TIME_DI with PEC controllers D512A
I would like to know if PEC PP D512 A it's compatible with Compact Control Builder 6.0 or under. I will need some special hardware to use TIME_DI or is done via software. Its possible to use without 800xa.
Voted best answer
Hi Marlon,
I've made some research and looks like PEC3 work only with Control Software 5.1.1-2 that's not exist for compact version.
For time_di my vest suggestion is try to change the OPCoDe to create this function using fast io.
Boa sorte,
Clayton
Add new comment