Cannot find logic in the program backup.
Hello
I got a program backup file from my client but the problem is,no logic or programming or code is there in the backup file.I've restored the backup file and opened it and I haven't get any code(logic) in the Program or diagram in the backup.Only the hardwere confugration is there.
The Logic backup is in Compact Control Builder AC800M,Version 5.0.1.0(Build 5.0.1001.75) System Version 5.0 SP1.
I've attached the logic,If it is possible to recheck the backup file wheather there is code(logic) or not it will be very helpfull for me.
As programming retrival is not possible from the system and I don't have proper backup so the only sollution is to recommission the system.
Please suggest.
Thank you
Voted best answer
Hello,
Also open the program by some manual work, both with ver. 5.0.1 and then 5.1.0.
It contains 4 controllers, running a control modules. No any code in the application.
Answers
Hello,
I was able to restore your project in Compact Control Builder 5.1 (sorry, don't have your version) without problems. It contained 4 applications with multiple control modules, so all code seems to be there.
Some questions which might help:
1. Did you restore the project from within Control Builder?
2. Did you restore from the zip-file or did you unpack it first? Try unpacking it manually in the project backup folder and then restore by selecting the .prj file.
3. Some zip programs/versions have problems with long file paths, the backup contains quite a long path: "Backup-When ABB NL left ship after service -30.05.2016"
Good luck
Add new comment