800xA History Server
Hi
Ist it possible to extend the live Trends and Eventlists on the productive System with the HistoryServer for 800xA Version 6.0.3.1?
Das anybody have one in central Europe?
See manual: 2PAA107563-600 B
Thanks Arno
Voted best answer
Yes, thats what it's build for. I assume you are using basic history. You can have both at the same time.
We use 800xA History several places (in england)
Pleace note the product did recieve several upgrade/bug fixes - So use 6.0.3 with History RU2.
The manuel you refer to is also rewised is now:
2PAA107563-600 D E en System 800xA 6.0 800xA History Administration and Configuration.
Answers
Do i have configure every single Signal or ist it like Audittrail with a Single Checkbox? I'm a confused about the License thing. We have around 20000 Tags with diffrent Alarms and Events. So i have to buy two of the 15,000 signals License?
Is maybe the IM a better and cheaper Solution if I would only extend the logs and the EventLists?
Is maybe the IM a better and cheaper Solution if I would only extend the logs and the EventLists?
Add new comment