System Event list - Invalid user Event.
What is the reason behind this type of event, the all the users are carefully configured per ABB documented procedure and this occurrence is random,
14-09-17 02:31:01:025 AspectDirectory_B60ASP012 Invalid user " " from node "B60OPW287B[AfwEventOPCServer,172.16.60.130]". B60ASP012
14-09-15 23:10:04:640 AspectDirectory_B60ASP012 Invalid user " " from node "B60OPW279S[AfwWorkplaceApplication,172.16.60.134]". B60ASP012
Any valuable suugestion is appreciated.
Voted best answer
These events are logged whenever the system is accessed from an account not defined in the 800xA User Structure.
The first seem to originate from unauthorized access to the 800xA OPC Event server while the second stem from some unauthorized workplace launch.
/S
Add new comment