Does AC 800F remember the configured IP address after wasEthernet board is changed?
Voted best answer
The answer is YES, the AC 800F CPU remembers the IP address, as long as the exchenged Ethernet board is set to '0'. In case the new ethernet board is set to e.g. 1 the saved IP address is overwritten, in this case by 172.16.1.1
Source: L4 support
Add new comment