Digivis Error Opening database (several instances)
Hello I am working with Windows Terminal Service to connect to PC with Digivis, I can open It without a problem, but when I run a second instance of Digivis (In local or remote) it gives me the fallowing error:
"Error On Opening database"
And on event viewer I can see the fallowing error:
Event Source:Freelance
Event Category:None
Event ID:1
Description:
Assertion failed: Fehler beim Oeffnen eines Superfiles! (OpenCtFile) at I:\DIGIMAT\KONF\DMB\SRC\DMBDB.C:624
I there a way to open a second instance of digivis as read only?
Voted best answer
Hi,
Second instance of opening DigiVis is not supported, instead you can use dual monitor configuration.
Add new comment