Error is importing Error from System 800xA 5.1 Rev A to System 800xA Rev D
I have installed New System 800xA System 800xA 5.1 Rev D and trying to import it's obejct type structre from my old backup which was on 800xA 5.1 Rev A
when i try to improt i recieve error that ABB 800xA system extension version 5.1.0-1 is missing but when i check i have base system 5.1.0-4 in installed softwrae but in Admin strrcutre in domian i can see base system 5.1.0
Anybody have idea ho wi can resolve this issue
screeshot of complete details attached for your review.
Answers
Hi
Just one try though there are less chances as the screenshot doesnot show any issues in installation and sys ext load
Did you load extensions successfully after installing 5.1 RevD?
If no, go to Configuration wizard and load the extension from Maintenance load
It should show a '*' also in front of ABB 800xA Base system extension in case maintenance load is pending
Hello,
Try this:
STEP 1) Go to SystemExtension; Select and right click; A pop up will appear; Select "No"
This will deregister the system extension. (Refer Pic)
STEP 2) Go to Admin Structure ->Administrative objects -> Inventory Object -> System Extension -> "ABB 800xA Base" Right click and delete it.
STEP 3) Go to Configuration Wizard; The Extension will be available to load again.
After loading your problem should be solved.
Hope it helps!!
Add new comment