Operator parameters for migration of CBF
Hi, In the context of revamping CBF V9.1 to CBF 2013, is it possible to load all of operator parameters (with yellow background) in a function of AC800F with CBF V9.1.
Regards,
Julien
Answers
Yes of couse, it is possible.
In Onlinemode, select a process station in the project tree and select load parameters in the menu bar.
You can select only the parameters with diffrences (standard view) and write this parameters back to the project file.
Also it is possible to export the parameter to a file.
Add new comment