How To upgrade AC160 with S800 and AF100 based IO to AC800M
I would like to kindly help me to upgrade attached configuration from AC160 to AC800M
Answers
http://www402.abbext.com/Advant-Contr...
The service is for AC450, but AC160 should be possible as most of the AMPL blocks and Database Elements are the same
BUT ......
This is not a completely Automated upgrade. The tool will help you convert the code, there is still a lot of engineering required.
Also, AC160 controller is for Power Applications so it may have special HMI display elements and connection to AC450. This is not a job for a beginner, but if you have good experience it should be possible.
Add new comment