How do i create a new SCD file for RTU560 from merged another SCD files
I have two ABB substations busbars ( 61850 REF560 relay and Unigear ZS2 cubicles) with two RTU 560 and each substation has an SCD file ( CEI61850). The two substations will be installed in a big substation wich will be controled by one RTU 560. I must merge two partial scd files to create a new complete scd file. How can i do it?
Answers
Hi,
There is SCD engineering tool called IET600 in ABB. In it create a new project and import the frist scd directly. In the same project, you create mulitple new IED's and import the content from second SCD one by one onto the new IED's using import option. The finallly make required configuration in this new project and export it as one single SCD.
Regards,
Santhanam
Add new comment