Digivis error massage "E_DMS_INSTALL_DOMAIN" for new installed Digivis in New OS windows 2000
Hi, the old OS computer became defected and I configure a new computer with new installed Widows 2000 and then I install Windows 2000 and Digivis V7.1 sp2 on the computer, All Network configuration such as IP, work group and ... is done according to old operator station computer.
when I connect it to ethernet network, the new configured computer could connect and identify successfuly in the ethernet network. (ping is OK and in CBF it can be identified with Version Error state).
in the CBF software "Version Error" appears for New OS computer.
then I try to perform "Whole Station" Download.
the download is in progress and when it reaches to 5% the below error massage appears:
"Load operation of object 543 failed due to error E_DMS_INSTALL_DOMAIN"
(as per attached picture)
I am sure that I didnt configure some program or setting for New OS computer.
could you please guide me how to solve the problem for New OS computer.
Thanks,
Best regards,
Answers
This question has not yet been answered.
Add new comment