ABB LICENSE ENTRY (VERSION 5.0.0.29) DO NOT HAVE "LICENSE/REQUEST SWKEY" SELECTION
when i install ABB CENTRAL LICENSING SYSTEM in stand-alone mode, set username to hostname\username, and set passwords to the same with username's .
when i finish the install process and open the ABB LICENSE ENTRY(VERSION 5.0.0.29), i found that there is not a selection of REQUEST SWKEY in menu LICENSE. So i can not get a license file (.sla) by license ID and machine ID, and i can not use the ABB software.
So i want to know why the ABB CLS don't have this selection, and how to get the license file by other methods?
Answers
License entry tool in stand alone installation also have a option in menu called Machine ID .
I hope this option is coming in your License Entry tool. If user select this option , a pop up will display availble machine id of system. Customer can request license based on this machine ID.
However if this option is not coming in your system , then the alternate way of requesting license is using MAC ID of System.
Go to Run>>CMD
in CMD prompt write >> ipconfig /all
the output of this command will display information related to ip configuration and MAC id details .
Note down the MAC ID of your control Network Adpater and request a license based on it.
Add new comment