AC800PEC
We are facing booting problem of AC800 PEC Controller, we tried to reset it through Recovery Procedure look like successful as manual.
After booting error message received as shown in attached pic-2.
As this case, we type: Reset in order to manual boot, same error information as auto reboot
Answers
Hello,
Looking from Pic2, PEC Controller boot was not successful. I hope you have proper tools such as Yellow color Cable and emulater Software like Tera Term or any Hyperterminal. Apart from this you need to follow follow PEC User manual.
Regards,
Shiv
Thanks Shiv Kumar,
We are using HyperTerminal and yellow cable. We are also following PEC Manual.
We start recovery procedure and results are according to manual, please find attached pics,
Abid Iqbal
Hello Abid,
Looks to be fine now. Now the PEC is in factory defualt stage with default IP address as shown in your attached Picture. Now next step, you need to load Firmware on the PEC Controller. Also you need to check if you need to change the IP Address of the PEC Controller. You can do simultaneously with the help of PEC Tool.
Regards,
Shiv Kumar
Dear Shiv Kumar,
We test Ping command but timeout and still there is same message after controller booting.
Hello,
Once your Controller in default IP, kindly chnage your PC IP similar to PEC Dafault IP. After that you can try with Ping Command. If still TimeOut persiste, kindly contact local ABB supportteam for resolution.
Regards,
Shiv Kumar
Add new comment